Types of Cable Armour
There are different materials used as cable armour to protect electrical cables. One type is AWA (Aluminium Wire Armoured) cable, which has aluminium wires applied to the bedding layer around the core for mechanical protection. Another type is SWA (Steel Wire Armoured) cable, which has a layer of galvanised steel wires applied to the bedding layer around the cores providing excellent protection against damage, impact, and corrosion. These materials depend upon the cable configuration, single or multicore.