Prysmian | Connectivity Portal

Video Library

A collection of several video guides and specific contents available to customers and installers.

Connectivity

How to Install Mini CSP

MMS

Datasheets

CMJ – COMPACT MULTI-FUNCTION JOINT®

MMJ – MEDIUM MULTI-FUNCTION JOINT®

LMJ – LARGE MULTI-FUNCTION JOINT®

SJC – SMALL JOINT CLOSURE®

UMJ – ULTRA COMPACT MULTI-FUNCTION JOINT®

PRECONNECTORISED UDS1 DROP CABLE®

PRECONNECTORISED 3mm DROP CABLE®

CBT – CASALINK BLOCK TERMINAL®

CASALINK BLOCK TERMINAL (CBT) DROP CABLES®

PRE-CONNECTORISED XMJ CLOSURE RANGE®

CCBT – COMPACT CASALINK BLOCK TERMINAL®

OPTITAP PRECONNECTORISED DROP CABLE®

HDB4 – HYBRID DROP BOX®

FLAT CTB – FLAT COMPACT TERMINATION BOX®

CBT EXTERNALCUSTOMER TERMINATION BOX MK1®

CTP – CUSTOMER TERMINATION POINT®

ACDC – AERIAL CONNECTORISED DROP CLOSURE®

mCSP – EXT MINI CUSTOMER SPLICE POINT

INTERNAL/EXTERNAL - SPLICE ONLY FLEXIBOX®

Question & Answer

A:  A range of integrated fibre management products for the deployment of an optical network, connecting head end active equipment to the end user/ consumer active equipment. Basically, it is the equipment that joins, terminates, and distributes optical cables. 

A:  Prysmian offers a full range of products from the central office to customer termination boxes. Within the Prysmian portfolio we have racks, Sub-racks/shelves/patch panels, closures, pre connectorized drop cables and wall boxes for internal and external applications. Prysmian also has a system for deploying fibres throughout a multi dwelling building, blown fibre and fibre to the room. 

A:  We have a range of test facilities within our factories that allow us to conduct thorough testing prior to launching any product to the market. We usually test to IEC standards but can test to Telcordia and some customers request specific tests. 

Some of the tests completed prior to product launch are: Change of temperature, Dry heat, Damp heat, Vibration, Shock, Impact, Ingress protection to name a few. 

A: An optical fibre is a thin, flexible filament of transparent material, usually glass, able to transmit light signals over long distances and at high speeds, averaging over 100 gigabits per second — like downloading an entire HD movie in one second.

The light travelling in the optical fibre is reflected by the fibre’s inner core, thereby maintaining its intensity and quality. In addition, the optical fibre is thinner than a human hair, with a diameter of about 0.1 millimetres. 

A: To enable its use, the optical fibre needs to be inserted inside an optical cable. To date, an optical cable can contain between 1 and 6,912 optical fibres and is designed to protect them adequately, also depending on where and how it is installed.

Contact Us