Hannover Building
Hannover Building
Hannover Square, Mayfair
The Hannover Square project in Mayfair was a significant undertaking, involving the installation of over 350,000 metres of Cat6a F/FTP Cca cable. This extensive cabling effort ensured robust and high-speed connectivity throughout the site. The project included the deployment of 5000 horizontal cabling outlets, strategically spread across low, mid, and high levels to cater to various connectivity needs.
In addition to the comprehensive cabling infrastructure, the project also saw the implementation of advanced fibre optic technologies. Both single-mode and multi-mode fibre optic technologies were utilised, providing versatile and high-performance data transmission capabilities. A total of 336 cores were installed, spanning over 25,000 metres in total length. This extensive fibre optic network was designed to support the demanding data requirements of modern applications, ensuring reliable and efficient communication across the entire site.
The meticulous planning and execution of this project highlight the commitment to delivering cutting-edge connectivity solutions, making Hannover Square a prime example of modern infrastructure development.