Fire Performance Cables
Prysmian Fire Performance (FP) Cables
Reliability at its core
The Fire Performance (FP) cable range is the result of over 50 years of continuous development of cables for fire alarms, emergency lighting, life safety and fire fighting systems. Prysmian FP cables are designed to maintain circuit integrity and continue to work for a specific time under defined conditions of 30, 60, or 120 minutes. Prysmian FP cables not only help save lives in a fire but also provide greater property protection.
Manufactured, certified and rigorously tested, FP cables undergo a range of fire tests to help protect both lives and property against fire. For common building applications, cables must meet minimum 30-minute flame tests with simultaneous impact and water spray. In contrast, large or complex buildings require cables to withstand higher temperatures and more demanding conditions for up to 120 minutes, ensuring safety remains uncompromised.
FP cables, the engineer's choice
For over 50 years, Prysmian has led the way in the researching and development of high-quality, reliable fire performance cables. This dedication to innovation began even before the establishment of British Standards for fire resistance, making Prysmian a trusted industry leader.
The Prysmian FP range remains the original choice for engineers - Independently tested and approved, FP cables are trusted across a range of fire-critical applications where safety and reliability are paramount.
To further support customers, Prysmian provides industry-leading seminars and technical resources, ensuring engineers have the knowledge and confidence to specify the right fire-resistant cables for every project. Learn more about why Prysmian FP cables set the standard for performance and safety here.
Fire Performance Cable Testing
The FP cable range undergoes rigorous testing to ensure the highest standards of safety and reliability. Located in Eastleigh, UK, the Prysmian fire testing laboratory operates full-time, conducting over 1,500 tests every year to refine existing cables and drive research and development into new solutions to meet future building regulations. This continuous dedication to innovation is a key factor that sets Prysmian apart.
These fire tests assess key elements like fire resistance, flame spread, and smoke emission, ensuring FP cables meet the toughest safety standards. This dedication to quality means FP cables don’t just tick the boxes – they help save lives and provide essential property protection when it matters most.
The FP cable range remains the first choice for engineers, installers, and regulators. Easy to install, fully compliant, and trusted in fire-critical applications, FP cables continue to set the highest standard for fire performance.


The FP cable range
Prysmian offers an extensive range of independently tested and certified fire resistant cables. The FP range meets the critical installation and performance criteria, delivering the highest possible quality standard. FP cables manufactured by Prysmian are designed to meet the requirements of the relevant fire tests.
'Standard' fire resistant cables are required to achieve at least 30 minutes circuit integrity when tested in accordance with BS EN 50200 AND also to BS EN 50200 ANNEX E. 'Enhanced' fire resistant cables are required to achieve at least 120 minutes when tested to BS EN 50200 AND also BS 8434-2. The Prysmian fire performance cable range includes FP100, FP200 Gold, FP400, FP PLUS and FP600s. Discover more about FP products below, or visit the FP product page for the full range.


Discover the FP cable range
The Prysmian fire performance cable range is the result of over 50 years of continuous development of cables for fire alarms, emergency lighting, life safety and fire fighting systems. Making them the ideal choice when choosing a reliable and trusted cable. Not only are they manufactured by Prysmian in the UK but they are also examined and certified to a range of tests that assess circuit integrity in the event of fire to help save lives and protect property.
FAQ
What are fire performance (FP) cables used for?
Toggle DetailsFire performance cables are used in essential systems such as fire alarms and emergency lighting, and critical life safety and fire-fighting systems to ensure circuit integrity in the event of fire. They are specifically designed to continue functioning under extreme conditions, helping to protect lives and property during emergencies.
Both cables meet the requirements of the relevant British Standards and are designed for different applications. In the event of a fire, FP PLUS cables last longer and at higher temperatures compared to FP200 Gold.
- FP200: Known as FP200 Gold, is a “Standard” fire resistant cable designed for fire detection, fire alarm and emergency lighting systems in buildings where minimum 30-minute fire resistance is required.
- FP PLUS: Designed for “Enhanced” fire resistance, FP PLUS is used in fire alarm and emergency lighting in hospitals and other large and complex buildings. FP PLUS is designed to keep circuit integrity for at least 120 minutes.
How long can FP cables maintain circuit integrity in a fire?
Toggle DetailsFP cables are designed to maintain circuit integrity for durations of 30, 60, or 120 minutes, depending on the application and risk assessment.


Power your success
Contact us
Select contacts by department