What is the maximum speed of fibre optic cable?
As the world becomes increasingly more connected, the need for reliable, faster fibre optic transmission speed remains paramount.
The Gigabit Britain rollout is currently underway. Since April 2026, around 90.5% of UK premises can now access gigabit-capable broadband, and the latest government target set out in the 2025 Spending Review is to reach 99% or premises by 2032.
- Fibre optic: up to 10Gbps (at a data transfer rate of up to 10 billion bits per second)
- Copper cable: 25-300 Mbps (at a data transfer rate of up to 300 million bits per second)
- DSL: 0.5-75 Mbps
- Satellite: 5-25 Mbps
What technologies can deliver Gigabit Broadband?
FTTP provides full fibre optic cable all the way from the nearest exchange point to the local roadside cabinet, achieving speeds from 40 Mbps to 1 Gbps.
How fast can fibre optic go?
Full fibre broadband is now available to over 90% of UK premises, with business users able to access speeds of up to 10Gbps and residential gigabit connections of 1Gbps now widely available across the country.
Since then, the record has been surpassed. In May 2025, researchers at the National Institute of Information and Communications Technology (NICT) and Sumitomo Electric achieved 1.02 petabits per second over 1,808 kilometres using a 19-core fibre with standard cladding dimensions.
What factors affect fibre optic speed?
Several factors can affect fibre optic cable transmission speed:
Bandwidth: This refers to the capacity of an internet connection that is shared by all users in a particular area. High usage by neighbours streaming films, attending Zoom meetings, or playing video games can reduce the available bandwidth and slow down internet speed for others.
Network congestion: During peak usage hours, more people are competing for the data, which can cause problems with bandwidth usage, leading to high latency. This means it will take longer for a particular amount of data to travel from one server to another. For internet users, it will take longer for a website to load, make online purchases, or watch a video.
Quality of equipment: The type and even the age of devices used can also have an impact. For example, types of hardware, network interface card (NIC), operating systems, and web browsers can all affect fibre optic speeds.
Single-mode vs multi-mode fibre: It is important to consider the type of fibre installed. Single-mode fibre is smaller in diameter but offers higher performance over longer distances. This is because there are lower internal reflections, which results in faster signals and a lower chance of signal loss. Multi-mode fibre has a larger diameter and experiences more internal reflections. This means the signal is slower and can only travel short distances.
What are the limitations of fibre optic?
Fibre offers higher bandwidth, faster speeds, longer transmission distances, and immunity to interference, but it is more expensive, fragile, and requires specialised installation. When installing fibre, extra care must be taken so that it is not twisted or bent too tightly. Copper is easier and cheaper to install, which makes it more suitable for shorter distances and less demanding applications, however, it has lower bandwidth, higher attenuation, and is susceptible to interference.
Prysmian Fibre Optic Cable: Linking the future
As demand for full fibre continues to rise, the transmission speed for fibre cable is continuing to increase, and Prysmian is constantly developing cable solutions that meet these evolving network demands.
From fibre optic and copper cables, to connectivity components and accessories; Prysmian is helping to link communities, continents and countries faster and more efficiently than ever before.